New at Mouser: Analog Devices / Maxim Integrated MAX96724/F/R Deserializer for ADAS Systems

New Product Press Brief

Connect With Us


May 18, 2023 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MAX96724/F/R GMSL2/1 to CSI-2 deserializer from Analog Devices / Maxim Integrated.

The Analog Devices / Maxim Integrated MAX96724/F/R quad-tunneling deserializers convert four GMSL™2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The MAX96724/F/R enables coexisting transmit bidirectional transmissions over 50Ω coax or 100Ω STP cables that meet the GMSL channel specification. Using industry-standard coax or STP interconnects, up to four remotely located sensors can be supported. Each GMSL2 serial link works at a fixed rate of 3Gbps or 6Gbps in the forward direction and 187.5Mbps in the reverse direction. The Analog Devices MAX96724/F/R enables aggregation and replicating video data, allowing streams from multiple remotely located sensors to be merged and routed to one or more available CSI-2 outputs.

These deserializer devices support high-bandwidth, gigabit multimedia serial links (GMSL-1 or GMSL-2) and offer spread spectrum and full-duplex control channel features.

Applications for the MAX96724/F/R deserializers include Advanced Driver Assistance Systems (ADAS) and other high-resolution camera systems.

To learn more, visit https://www.mouser.com/new/analog-devices/maxim-max96724-f-r-deserializers/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764