Mouser Now Stocking Analog Devices AD9081 & AD9082 MxFEs for Broadband Communications and Wide-Bandwidth Signal Processing
July 22, 2021 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now shipping the AD9081 and AD9082 mixed-signal front-ends (MxFE™) from Analog Devices, Inc. The two versatile RF converter platforms combine high-performance analog and digital signal processing for wireless applications, including 4G LTE and 5G millimeter-wave (mmWave) radios as well as phased array radar systems and electronic defense applications.
The Analog Devices AD9081, available from Mouser Electronics, is a reconfigurable, highly integrated RF MxFE that incorporates four 16-bit, 12 GSPS digital-to-analog (DAC) cores and four 12-bit, 4 GSPS analog-to-digital converter (ADC) cores. Eight transmit and eight receive lanes provide 24.75 Gbps/lane at JESD204C, or 15.5 Gbps/lane at JESD204B. The AD9081 is available in two models: the 4D4AC model supports full instantaneous channel bandwidth, and the 4D4AB model provides maximum fast bandwidth at 600 MHz per channel, with automatic configuration of the digital signal processor (DSP) to limit bandwidth at startup.
The AD9082 MxFE integrates four 16-bit, 12 GSPS DAC cores and two 12-bit, 6 GSPS ADC cores, with support for eight transmit and eight receive lanes, providing 24.75 Gbps/lane (JESD204C) or 15.5 Gbps/lane (JESD204B). The AD9082 is also available in two models — the 4D2AC model, which supports four DACs and two ADCs, and the 2D2AC model, which supports two DACs and two ADCs. Both MxFEs feature an on-chip clock multiplier and DSP and offer a bypass mode to allow the ADC or DAC cores’ full bandwidth capability to bypass DSP data paths.
The AD9801 and AD9802 are supported by the AD9081-FMCA-EBZ and AD9082-FMCA-EBZ evaluation boards, respectively, which include all support circuitry required to operate the MxFEs in various modes and configurations. The eval boards connect to the ADI ADS9-V2EBZ or the ADS8-V3EBZ (sold separately) for evaluation with the ADI Analysis | Control | Evaluation (ACE) software, and can also interface with FPGA development boards from Xilinx® or Intel®.
To learn more about the AD9081 MxFE, visit https://www.mouser.com/new/analog-devices/adi-ad9081-adcs/. For more information about the AD9082 MxFE, go to https://www.mouser.com/new/analog-devices/adi-ad9082-mxfe/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.
Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - Analog Devices, Inc. operates at the center of the modern digital economy, converting real-world phenomena into actionable insight with its comprehensive suite of analog and mixed signal, power management, radio frequency (RF), and digital and sensor technologies. ADI serves 125,000 customers worldwide with more than 75,000 products in the industrial, communications, automotive, and consumer markets. ADI is headquartered in Wilmington, MA. Visit http://www.analog.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.