Arduino’s Opta Micro Programmable Logic Controllers, Now Available at Mouser, Enable Industrial IoT Applications
May 15, 2023 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Opta® micro programmable logic controller (PLC) from Arduino. The easy-to-use controller allows designers to scale industrial automation projects using the open Arduino ecosystem. The Opta PLC supports real-time control, monitoring, and predictive maintenance, making it an ideal choice for Industrial Internet of Things (IIoT) and building automation applications.
The Arduino Opta micro PLC, now available at Mouser, is based on the STM32H747XI dual-core microcontroller from STMicroelectronics, which includes a single high-performance Arm® Cortex®-M7 core running at up to 480 MHz and a lower-power Cortex-M4 core running at up to 240 MHz alongside a shared floating-point unit (FPU).
The Opta is offered in three variants:
- Opta Lite, which includes Ethernet connectivity and USB Type-C™ for programming
- Opta RS485, which adds RS485 half-duplex support
- Opta WiFi, which includes radios for Wi-Fi® and Bluetooth® Low Energy (BLE) connectivity
All models support over-the-air updates and feature a dedicated secure element for cryptographic assurances, plus relays for switching four loads of up to 2.3 kW each. The highly versatile controllers also include optional support for standard IEC 61131-3 PLC languages and fieldbus integration via Modbus TCP and Modbus RTU.
The Opta PLCs were recently featured in a Mouser Webinar. Featuring two expert panelists from Arduino, the video webinar provides device designers with everything they need to know to develop and scale their industrial automation projects.
To learn more about the Opta micro programmable logic controllers, visit https://www.mouser.com/new/arduino/arduino-opta-micro-plcs/.
To view the Mouser Webinar Scale Up Automation with the new Arduino Opta microPLC, visit https://resources.mouser.com/mouser-webinars/scale-up-automation-with-the-new-arduino-opta-microplc/
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.
Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - Arduino (a Qualcomm Technologies, Inc. company) is a leading open-source hardware and software provider and an accessible platform for creating interactive projects. With an estimated 33 million active users, the Arduino ecosystem has expanded over 20 years to address new demands and challenges, offering products for IoT, wearables, 3D printing, and embedded environments. With the Pro range, Arduino supports companies that are interested in going beyond the concept and rapid prototyping phase, to start mass production with the support of a qualified industrial partner and high-performance technological solutions.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.