Mouser Electronics and Diotec Semiconductor Announce Global Distribution Agreement

For Immediate Release

Connect With Us


June 20, 2022 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, announces a global distribution agreement with Diotec Semiconductor, designers and manufacturers of discrete semiconductor components. According to the agreement, Mouser will offer customers Diotec Semiconductor’s range of diodes, rectifiers, FETs, and voltage regulators for commercial- and industrial-grade applications.

The CL15M45/CL20M/CL40M45 SMD current-limiting diodes deliver parallel operation for higher current intensity (IP), providing a durable, high-performance solution for applications such as low-power LED drivers and battery chargers. Offering 1 W power dissipation, 0.5 V reverse voltage, and an operating junction temperature of -50°C to +150°C, the current limiting diodes provide commercial-grade performance in an SMB package.

The MMBT7002K N-channel enhancement mode FETs deliver exceptional performance for signal processing, logic level converter, and driver applications. The FETs offer ESD-protected gate fast switching times, as well as an operating junction temperature of -55°C to +150°C. The MMBT7002K FETs feature 350 mW power dissipation, 20 V gate-source voltage, and 60 V drain-source voltage.

Diotec Semiconductor’s BAV99x small-signal diodes deliver high switching speeds with low junction capacitance and low leakage current. The BAV99x diodes are built with UL 94V-0 case materials, and devices with an -AQ suffix in the product number have achieved AEC-Q101 qualification. The diodes support a range of applications, including signal processing, rectifying, and high-speed switching.

The EGL1x superfast recovery rectifiers feature an impressive reverse voltage (VR) range of 50 V to 400 V and 50 V to 400 V peak repetitive reverse voltage (VRRM). These high-performance diodes offer high power dissipation and enable rectification of high frequencies.

To learn more about Diotec Semiconductor products available from Mouser, visit https://www.mouser.com/manufacturer/diotec-semiconductor/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Diotec Semiconductor

2026 - Diotec Semiconductor specializes in the design and manufacturing of discrete semiconductor components. Diotec diodes, bipolar junction transistors, MOSFETs, and linear voltage regulators address a wide diversity of applications, ranging from industrial and automotive to consumer electronics. Founded in 1973 in Heitersheim, Germany, Diotec has since expanded to four manufacturing locations on three continents.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764