Ezurio's Vela IF310 Multiprotocol Modules, Now at Mouser, Feature Next Gen Audio-Centric Bluetooth Core 6.0 Classic and LE Connectivity

New Product Announcement

Connect With Us


Learn more about the Vela IF310 modules
Learn more about the Vela IF310 modules

May 20, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Vela™ IF310 multiprotocol modules from Ezurio. The Vela IF310 modules are based on the Infineon Technologies AIROC™ CYW55310 system on chip (SoC) and combine Bluetooth® Classic (BR/EDR) and the complete Bluetooth 6.0 Low Energy (LE) feature set. Engineered for high-reliability environments, the Vela IF310 modules deliver a low-risk, fast-to-market platform for applications including fitness equipment, automotive infotainment, POS and barcode scanners, and medical monitors.

The Ezurio Vela IF310 modules, now at Mouser, include LE audio with LC3, isochronous channels, Auracast, LE-coded, and two MPHY and advertising extensions, allowing legacy classic designs to be updated with a single module. The Vela IF310 modules feature a powerful MCU subsystem with a 192 MHz Arm® Cortex-M33 processor, 2 MB ROM, and 768KB SRAM, with TrustZone® and CryptoCell™-312 security. The Vela IF310 series also offers a rich set of audio interfaces, including dual TDM/I2S plus PCM for HFP, A2DP, LE Audio, and multi-stream use cases. With flexible software hosting, the modules can be seamlessly integrated into automotive, retail, and medical applications. The Vela IF310 modules offer a single 12 × 16 mm2 footprint with multiple antenna variants, including integrated Ignion antenna, MHF4 connector, or RF trace pad, along with DVKs to make it easy to evaluate in real-world environments. The Vela IF310 modules minimize downtime in clinical settings and ensure interference-resistant audio in industrial spaces, with a rugged operating temperature range of -40°C to +85°C.

Ezurio Vela IF310 development kits provide a platform for rapid development and testing of the Vela IF310 modules. Two variations are available: part # 453-00390-K1 features an integrated chip antenna, and part # 453-00391-K1 includes an MHF4 connector for an external antenna. Featuring on-board headers and jumpers, the development kits provide a convenient way to isolate power and signal nets for debugging and power measurements.

To learn more, visit https://www.mouser.com/new/ezurio/ezurio-vela-if310-modules/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Ezurio

2026 - Ezurio turns design possibility into reality with a comprehensive range of RF modules, system-on-modules, single-board computers, internal antennas, IoT devices, and custom solutions. With decades of engineering expertise, Ezurio provides solutions that reduce development costs and time to market. Ezurio's global reach and unmatched support are backed by a resilient global supply chain that gives our customers the stability to overcome every design challenge with confidence. Turn design possibility into reality with Ezurio, your connectivity expert.

Laird Connectivity and Boundary Devices are now Ezurio.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764