Now at Mouser: Monolithic Power Systems (MPS) MPQ4242B-AEC1 Fully Integrated Power Delivery IC for Automotive Applications

New Product Announcement

Connect With Us


Learn more about the MPQ4242B-AEC1 PD IC
Learn more about the MPQ4242B-AEC1 PD IC

May 12, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the MPQ4242B-AEC1 fully integrated power delivery (PD) IC from Monolithic Power Systems (MPS). The MPQ4242B-AEC1 features an integrated buck-boost converter with four power switches and a USB PD controller. The MPQ4242B-AEC1 is AEC-Q100 Grade 1 qualified and designed for USB Type-C® sourcing ports in automotive applications.

The Monolithic Power Systems (MPS) MPQ4242B-AEC1 PD IC, now available at Mouser, supports up to 5-amps of continuous output current (IOUT) over the specified input supply range. The MPQ4242B-AEC1 features a USB Type-C port that supports USB PD revision 3.1 with a programmable power supply (PPS). The MPQ4242B-AEC1 is backward-compatible with dedicated charging port (DCP) schemes for battery charging specification (BC1.2), 3A divider mode, and 1.2V/1.2V mode. In addition, the MPQ4242B-AEC1 supports QC 2.0/3.0 and the Huawei Fast Charge Protocol (FCP) mode. When battery voltage (VBATT) is low or in the event of over-temperature (OT), the MPQ4242B-AEC1 provides a configurable PD power management state machine.

The MPQ4242B-AEC1 also includes fault condition protections, including input/output (I/O) pin short protection for the BUS and VIN pins, CC overcurrent protection (OCP), current limiting with hiccup mode, output overvoltage protection (OVP), and thermal shutdown. The MPQ4242B-AEC1 is delivered in a QFN-22 (4 x 5 mm2) package and requires readily available, standard external components.

The MPS EVQ4242B-VE-00A evaluation board, also available from Mouser, provides a demonstration and development platform for the MPQ4242B-AEC1. The evaluation board features a pre-mounted MPQ4242B-AEC1, along with the required components and headers enabling access to key signals. The EVQ4242B-VE-00A evaluation board provides an example application circuit, allowing rapid prototyping when incorporated into existing designs.

To learn more, visit https://www.mouser.com/new/monolithicpowersystems/mps-mpq4242b-aec1-power-delivery-ic/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Monolithic Power Systems (MPS)

2026 - Monolithic Power Systems (MPS) provides small, highly energy-efficient, easy-to-use power solutions for systems found in industrial applications, telecom infrastructures, cloud computing, automotive, and consumer applications. MPS creates cutting-edge solutions to improve the quality of life with green, easy-to-use products.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764