NXP Semiconductors i.MX 91 Processors, Now Available from Mouser Electronics, Support IoT, Edge, Smart Home, Industrial Applications, and More

New Product Announcement

Connect With Us


Learn more about the i.MX 91 Processors
Learn more about the i.MX 91 Processors

February 17, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new energy-efficient i.MX 91 applications processors from NXP® Semiconductors. The i.MX 91 processors enable the rapid development of Linux-based edge devices for smart home, consumer, industrial, and medical applications.

The NXP Semiconductors energy-efficient i.MX 91 system-on-chips (SoCs), available from Mouser, are high-performance, affordable, secure solutions for evolving protocols and emerging standards. The i.MX 91 family is part of the i.MX portfolio of applications processors, featuring an Arm® Cortex®-A55 running at up to 1.4 GHz, support for platform longevity with LPDDR4 memory, dual Gigabit Ethernet ports, dual USB ports, and a rich set of peripherals. Supported by NXP's product longevity program, the i.MX 91 SoCs, integrated with EdgeLock® Secure Enclave (Advanced Profile), supply security features, including lifecycle management, tamper detection, secure boot, and a simplified certification path with consumer/industrial qualifications, targeting the medical, industrial, and consumer IoT market segments.

Mouser also stocks the NXP Semiconductors FRDM-IMX91S development board, which is designed to evaluate the i.MX 91 applications processor for Linux®-based edge devices. The FRDM‑i.MX 91S integrates an NXP PF9453 PMIC and an IW610‑based tri‑radio module providing Wi‑Fi® 6, Bluetooth® LE 5.4, and IEEE 802.15.4 connectivity. It includes support for Yocto‑based Linux and Debian images. It includes 256 MB NAND with direct NAND boot and a lightweight, reliability‑tuned filesystem that minimizes resources—its small footprint maximizes usable storage and keeps operation efficient. This development board is also designed for entry-level Linux® use-case evaluation, enabling developers to accelerate product development while significantly reducing costs.

The NXP Semiconductors i.MX 91 Evaluation Kit, available from Mouser, is designed for evaluating i.MX 91 processor applications and measuring power consumption on power rails. The NXP Semiconductors i.MX 91 kit consists of two interconnected boards: a compute module and a connectivity baseboard. The compute module, built with standard 6-layer technology, features an i.MX 91 SoC, 2GB LPDDR4, 16GB eMMC, NXP's PMIC (PCA9451A), and power monitoring circuits. The connectivity baseboard features a standard M.2 KEY-E slot, enabling off-the-shelf connectivity modules, including Wi-Fi and Bluetooth connectivity via the NXP IW610 module. It includes the GoPoint application, which allows designers to explore pre-installed demos, providing an excellent foundation for accelerating design development.

To learn more, visit https://www.mouser.com/new/nxp-semiconductors/nxp-imx-91/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764