TDK's FS1525 25A Stackable µPOL Regulator, Now at Mouser, Provides up to 200A in Vertical Power Delivery Designs

New Product Announcement

Connect With Us


Learn more about the FS1525 µPOL regulator
Learn more about the FS1525 µPOL regulator

April 30, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the FS1525 25A stackable µPOL regulator from TDK. The FS1525 is an easy-to-use, fully integrated, and highly efficient micro-point-of-load (µPOL) voltage regulator. The regulator is engineered to meet the demands of AI servers, data center systems, edge computing, telecom and networking, industrial applications, and distributed point-of-load (PoL) power architectures.

The TDK FS1525 µPOL regulator, now available at Mouser, delivers 25A per module and up to 200A when stacking multiple units in vertical power-delivery designs. The ultra-compact, accurate regulator features an on-chip pulse-width modulation (PWM) controller, integrated MOSFETs, along with an incorporated inductor and capacitors. The FS1525 offers built-in protection, including pre-biased start-up, soft-start protection, thermally compensated overcurrent protection with hiccup mode, overvoltage protection, and thermal shutdown with auto-recovery. It also features ultra-fast transient response, ultra-low DC ripple, and true differential remote sensing for accurate voltage regulation at the point of load.

The TDK FS1525 provides programmable operation via I2C and PMBus protocols, enabling real-time telemetry, adaptive tuning, and fault management for voltage, current, and temperature monitoring. The compact, low-profile regulator measures 6.80mm x 7.65mm x 3.82mm and is suitable for automated assembly using standard-mount equipment. The FS1525 offers a plug-and-play design and requires no external components, simplifying designs, accelerating development, and reducing overall system costs.

The TDK EV1525-0800-25A/-50A/-100A µPOL evaluation boards help start development with the FS1525 regulator. The evaluation boards produce an output voltage (VOUT) of 0.8V for loads of 0A to 25A (EV1525-0800-25A), 0A to 50A (EV1525-0800-50A), or 0A to 100A (EV1525-0800-100A) from an input voltage (PVIN) of 12V.

To learn more, visit https://www.mouser.com/new/tdk/tdk-fs1525-upol-regulators/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About TDK

2026 - TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately "Attracting Tomorrow." It was established in 1935 to commercialise ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminium electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. 

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764