New Interactive eBook from Mouser and TDK Explores Challenges in Precision, Speed, and Efficiency for Industrial Automation

For Immediate Release

Connect With Us


June 5, 2025 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, announces a new interactive eBook in collaboration with TDK, one of the world's largest electronic components manufacturers, exploring the challenges of efficiency, safety, and sustainability in advanced automation applications.

Modern Industrial Technologies: Driving Efficiency and Innovation gives a deep dive into the ever-increasing demands for precision, speed, and efficiency in modern industrial automation, robotics, energy and sensor technology and how TDK's technology portfolio empowers engineers to overcome these challenges. With TDK's solutions already deployed across multiple industrial automation disciplines, this eBook gives insights into various considerations vital to a whole range of automation activities, from simple voltage and current measurements to complex navigational signal analysis and system diagnostics. The eBook highlights many of TDK's products that help bridge these challenges:

The ERUC23 SMT flat wire coupled inductors feature low-loss ferrite, high-saturation currents, and low DC resistance, offering self-leaded construction with flat wire winding and lead-free tinned terminals for 48Vinto 12Vout hybrid converters and dual-phase buck, boost, and buck-boost converters. The ERUC23 inductors also provide reduced ripple with improved efficiency in a compact package. The ERUC23 series is RoHS compatible and AEC-Q200 qualified.

The B43659 ultra-compact snap-in capacitors provide high reliability and high ripple current capability for power supplies, frequency converters, uninterruptible power supplies (UPS), medical appliances, and solar inverters. These extremely high CV products feature snap-in solder pins, an aluminum case, and both two-terminal and three-terminal versions to ensure correct installation. The B43659 series is RoHS compliant and offers a rated voltage of 450VDC and a capacitance range of 140µF to 1030µF with ±20% tolerance and operating in a -40°C to +105°C temperature range.

EPCOS / TDK's PiezoHapt™ and PowerHap™ actuators are ideal for providing haptic feedback to user actions in smartphones and touchpad displays, car navigation systems, controllers, household appliances, industrial equipment, and medical devices. The PiezoHapt actuators consist of a vibration unit with a multilayer piezoelectric element and vibration plate, while the PowerHap version has multilayer piezo plates with copper inner electrodes. These devices are RoHS compatible and have an operating temperature range of -10°C to +60°C or -40°C to +85°C.

The FLECLEAR Ag-Stacked Film Sheets feature a thin, transparent, conductive Ag alloy layer that is deposited on a film substrate, ideal for light control windows (smart windows) and organic photovoltaics (OPVs), flexible displays and lighting, or transparent electrodes of wearable devices.

To read the new interactive e-book, visit https://www.mouser.com/tdk-transforming-industries-ebook/. To learn more about all the TDK products available from Mouser, visit https://www.mouser.com/manufacturer/tdk-corp/.

To browse Mouser's extensive eBook library, visit https://resources.mouser.com/manufacturer-ebooks/

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About TDK

2026 - TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately "Attracting Tomorrow." It was established in 1935 to commercialise ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminium electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. 

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764