Mouser Now Stocking the TE Connectivity Heavy-Duty Sealed Connectors with MATEnet Inserts for Ethernet+Power Transmission

New Product Announcement

Connect With Us


November 21, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the Heavy-Duty Sealed Connectors with MATEnet Inserts from TE Connectivity. Taking advantage of the rugged reliability and scalability of the company's heavy-duty sealed connector series housings, TE Connectivity has leveraged this technology with high-performance MATEnet inserts to offer designers a versatile connector that incorporates power and Ethernet connectivity up to 1 Gbps for use in heavy-to-medium-duty trucks, buses, agricultural machinery, construction and other commercial vehicle applications.

The TE Connectivity Heavy-Duty Sealed Connectors with MATEnet Inserts, available from Mouser Electronics, are highly adaptable and modular Ethernet connector solutions made to fit a variety of customer needs for data and power transmission applications in the industrial automotive market. These hybrid signal-to-power connectors are designed to perform in very tough and harsh environments and provide designers the flexibility of wire-to-wire, wire-to-device and wire-to-board configurations. Scalable for use with jacketed unshielded twisted pair (UTP) and shielded twisted pair (STP) cables, the highly conformable design of these connectors also supports tab housing options for in-line and panel-mount applications, along with standard 180° and 90° header selections.

Regarding Ethernet and communication capabilities, these Heavy-Duty Sealed Connectors help meet current and future data requirements by enabling speeds from 100 Mbps to 1 Gbps, being fully compliant with industry-standard protocols IEEE802.3bw, 100BASE-T1 and 1000BASE-T1. Based on application requirements, these connectors also support hybrid design options for multiple Ethernet ports and power pin configurations with numerous wire sizes to expand usage opportunities.

TE Connectivity's Heavy-Duty Sealed Connectors with MATEnet Inserts are available in a rugged package that is IP67 and IP69K (with backshell) rated for dust and water protection, vibration and mechanical shock resistant and securely connected utilizing a built-in secondary locking feature for contact retention. The connectors are specified at an industrial temperature range of -40°C to +125°C (cable dependent), and target industrial applications include network backbones, sensors, camera systems, sealed controllers, gateways/switches, radar/LiDAR, and in-cabin and automotive chassis.

To learn more, visit https://www.mouser.com/new/te-connectivity/te-heavy-duty-connectors-matenet-inserts/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About TE Connectivity

2026 - TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions, proven in the harshest environments, enable advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With more than 85,000 employees, including over 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764