Authorized Distributor Mouser Electronics Shipping Wide Variety of Electronic Components and Semiconductors from Toshiba

For Immediate Release

Connect With Us


September 5, 2024 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is an authorized global distributor of electronic components and solutions from Toshiba. With over 7,000 Toshiba products available to order, including over 3,000 in stock, Mouser offers a wide portfolio of the newest Toshiba components to help buyers and engineers bring their products to market.

The Toshiba TCKE9 Series 23V 4A eFuse ICs, available from Mouser, are electronic fuses that protect power supply lines from external overcurrent and overvoltage. The TCKE9 Series products have an adjustable current limit and fixed voltage clamp functions, in addition to slew rate control, UVLO, FLAG output, and more. eFuses offer repeatable protection and great accuracy, which is something that standard physical fuses do not.

The UMOS9-H silicon N-channel MOSFETs from Toshiba are ideal for high-efficiency DC-to-DC converters, switching voltage regulators, and motor drivers. Based on a next-generation U-MOS9-H trench process, these MOSFETs deliver high efficiency at all loads. These devices feature 80V drain-source voltage, ±20V gate-source voltage, and 175°C channel temperature. The UMOS9-H MOSFETs are available in a DPAK package option that realizes low on resistance (RDS(ON)) and low output charge (QOSS) for increased efficiency in switching-mode power supplies used in base stations, servers, or industrial equipment.

Toshiba's 40V and 50V fully integrated stepper motor drivers exhibit low on-resistance, fine micro-stepping, and compact form factor with motor driving enhancement features that are suitable for a wide range of industrial applications like actuators and CNC machines. These devices enable a motor to be driven by a single VM power supply with a built-in regulator for IC operation.

The TLP2362B, TLP2368B, TLP2762B, and TLP2768B high-speed isolated photocouplers support and handle slow inputs that add unwanted chattering noise. These devices simplify design and eliminate required external components like Schmitt triggers, which are traditionally used to reduce chattering noise. These photocouplers integrate an internal Faraday shield that provides a guaranteed common-mode transient immunity of ±50 kV/µs. They are well suited for programmable logic controllers, factory automation, and test and measurement equipment.

To learn more about Toshiba, visit https://www.mouser.com/manufacturer/toshiba-semiconductors/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Toshiba

2026 - Toshiba Electronic Devices & Storage Corporation (TDSC) offers a broad IC and discrete product line-up which includes Power, Small Signal, Optoelectronics, and Logic devices for automotive, multimedia, industrial, telecoms, and networking applications. TDSC develops, manufactures, and supplies innovative storage products including Enterprise and Consumer HDDs.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764