New at Mouser: Vishay VS-HOT200C080 200A 80V Power MOSFET Module for MHEV and Micro Mobility Applications

New Product Announcement

Connect With Us


Learn more about the VS-HOT200C080 Power MOSFET module
Learn more about the VS-HOT200C080 Power MOSFET module

October 7, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new VS-HOT200C080 200 A, 80 V Power MOSFET module from Vishay Intertechnology. The VS-HOT200C080 is an integrated device that saves space, reduces conduction losses, and increases reliability for 48 V traction inverters in light electric vehicles (LEV) and belt-start generator/recuperation systems for mild-hybrid electric vehicle (MHEV) applications.

The Vishay VS-HOT200C080 Power MOSFET module, available from Mouser, integrates 80 V MOSFETs in a half-bridge configuration, with best-in-class RDS(ON) in a compact transfer-mold FlatPAK HC0 package. In addition, the VS-HOT200C080 features a shunt resistor for current reading, bypass capacitors for improved switching performance, and an NTC for temperature sensing. To increase efficiency, the low on-resistance of the MOSFET reduces conduction losses by 32% compared to competing solutions, plus reduces board space requirements by up to 15% compared to standard discrete solutions. This device has a drain-to-source voltage (VDSS) of 80 V and a continuous drain current (ID) of 195 A (TC = +80°C). The power module's transfer-mold technology enables highly reliable performance over a wide operating temperature range from -55 °C to +175 °C, especially during power cycling, allowing the device to meet severe AQG-324 reliability requirements.

The VS-HOT200C080's HC0 package also features signal pins and power tabs at different heights. This allows designers to use separate power and signal PCBs, simplifying designs and enabling better routing. To save additional board space, the signal and power PCBs can be stacked.

To learn more, visit https://www.mouser.com/new/vishay/vishay-semi-vs-hot200c080-power-mosfet-module/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Vishay

2026 - Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764