WiFi and Bluetooth Coexist with the Atmel WINC1500 Low Power WiFi Module Now at Mouser
March 12, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now shipping the new WINC1500 Wi-Fi Module from Atmel Corporation. The WINC1500 is a low-power consumption 802.11 b/g/n WiFi module specifically optimized for low power Internet of Things (IoT) applications. The WINC1500 WiFi module supports WEP, WPA, and WPA2 WiFi security encryption as well as China WAPI security while drawing as little as 4µA. This module includes features that allow both WiFi and Bluetooth signals to coexist locally without any signal interference.
The Atmel WINC1500 Wi-Fi Module, available from Mouser Electronics, is a highly integrated device featuring a small form factor at only 21.5mm x 14.5mm x3.4mm. This module includes an integrated power amplifier, low noise amplifier (LNA), all necessary power management functions, and an integrated antenna. This module targets low power WiFi wireless applications and draws only 4µA in Deep Power Down mode. When in beacon monitoring mode the module draws only 850µA in Doze Mode. This module provides SPI, UART, and I2C host interfaces for communicating with a host microcontroller. It also supports 2-wire and 3-wire Wi-Fi/Bluetooth coexistence signaling interface. The interface allows this module to coordinate transmission and reception with a compatible Bluetooth module to insure that both radios do not interfere with each other.
The Atmel WINC1500 is based on a powerful Cortus-APS3 32-bit processor. This processor performs hardware accelerated MAC functions including association, authentication, power management, security key management, and MSDU aggregation/de-aggregation. In addition, the processor provides flexibility for various modes of operation, such as STA and AP modes. An on-chip IP stack minimizes the host microcontroller requirements and supports TCP, UDP, DHCP, ARP, HTTP, SSL, and DNS.
To learn more, visit: http://www.mouser.com/new/atmel/atmel-winc1500/ .
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.
Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - Atmel Corporation is a global leader in designing, manufacturing and marketing advanced semiconductors including microcontroller (MCU), programmable logic, and nonvolatile memory. By combining these core technologies, Atmel meets the evolving and growing needs of today's electronic system design engineer through the production of general purpose and application specific system level integrated chips. Atmel's world class expertise and wealth of experience in system-level integration enable all of Atmel's products to be developed from their constituent blocks with minimum delay and risk.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.