Now at Mouser: HARTING’s Standard-Setting T1 Industrial Single Pair Ethernet Products
August 20, 2020 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking T1 Industrial single pair Ethernet (SPE) products from HARTING. Selected by the International Electrotechnical Commission (IEC) as the standardized SPE mating face (IEC 63171-6), HARTING's innovative T1 Industrial products enable transmission of data via Ethernet using just two wires, and also offer simultaneous power supply for terminals using Power over Data Line (PoDL).
HARTING T1 Industrial SPE products, available from Mouser Electronics, allow barrier-free connection of sensors, equipment, and actuator technology into the field level using end-to-end IP-based communications, delivering new space and power efficiencies for a range of industrial and communications applications. The products boast a robust industrial design with locking lever protection, high mating cycles, and 360-degree shielding. In addition to the IEC 63171-6 standardized mating face, these T1 Industrial products also meet cabling standards according to ISO/IEC 11801 and TIA 42.
The new devices support the construction of future-proof SPE communication networks, while also offering remote power supply for all PoDL classes. T1 Industrial SPE products simplify parameter setting, initialization, and programming of communication networks, while simultaneously improving the efficiency of equipment set-up, operation, and maintenance.
To learn more about the T1 Industrial SPE Products, visit https://www.mouser.com/new/harting/harting-t1-industrial/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser is a leading authorised distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in Stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in Stock for immediate shipment.
Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - HARTING is the gold standard in connectivity for industrial environments and mission-critical applications. As the pioneer in connectivity, HARTING combines the quality and customer service of its family-owned operations with a global footprint backed by in-region manufacturing facilities and local teams with deep engineering expertise.
With a reliable and robust approach to connectivity for any environment, HARTING enables improved efficiency and sustainability and future-proofs the businesses of today to power the innovations of tomorrow.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.