Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Marvell Alaska Multi-Gigabit Ethernet Transceivers Now Shipping from Mouser Electronics

September 18, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking an expanded selection of Alaska® Ethernet transceivers from Marvell Semiconductor.

The Alaska C 88X5113 Ethernet transceiver is a fully integrated Ethernet transceiver that performs the Gearbox functionality required to translate from 40G Ethernet to 25G Ethernet. The device, fully compliant with the IEEE 802.3by 25GbE and 802.3bj 100GbE standards, enables design engineers to support IEEE 25GbE specifications on their existing switch ASICs without the expensive investment involved in new silicon development.

Alaska M 88E2010 and 88E2040 devices are octal Multi-Gigabit Ethernet transceiver compatible with both IEEE 802.3bz standard and NBASE-T Alliance specification for 2.5 and 5 Gbps operation over CAT5e cables. The devices support Category 6 (screened or unscreened), Category 6a (augmented) and Category 7 type cables, as well as Category 5e type cables for distances up to 100 m. The devices also support a variety of host interfaces (2500BASE-X, 5000BASE-R, SGMII), as well as 10G host interfaces such as USXGMII interface and XFI/RXAUI with Rate-Matching. The transceiver family also features full backward compatibility with lower-speed legacy Ethernet (1000/100/10 Mbps) on the line side.

The Alaska X 88X2222 and 88X2242 transceivers are fully integrated single-chip solutions that providing end-to-end data transmission over fiber-optic networks as well as Twinax copper links. The 88X2222 device supports two ports of 10G SFP+ connectivity, while the pin-compatible 88X2242 is designed to deliver support for one port of 40G QSFP+ or four ports of 10G SFP+ Ethernet connectivity. The devices offer ultra-low-latency, wire-speed encryption for security and high reliability with port failover mechanisms.

To learn more about the Marvel Alaska C family, visit www.mouser.com/marvell-alaska-c-transceivers. For more information on the Alaska M family, go to www.mouser.com/marvell-alaska-m-phys. To learn more about the Alaska X family, visit www.mouser.com/marvell-alaska-x-transceivers.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 26 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Marvell Semiconductor
Marvell first revolutionized the digital storage industry by moving information at speeds never thought possible. Today, that same breakthrough innovation remains at the heart of the company's storage, networking, and connectivity solutions. With leading intellectual property and deep system-level knowledge, Marvell's semiconductor solutions continue to transform the enterprise, cloud, automotive, industrial, and consumer markets.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room