Accurate depth measurement is a fundamental requirement for modern autonomous systems, yet achieving precision across varying ambient lighting conditions remains a significant challenge. Whether a robot is navigating a cluttered warehouse or a camera system is attempting to focus on a fast-moving subject, the ability to distinguish between objects at different distances is critical. Traditional proximity solutions often struggle with “ghost targets” and environmental interference, which can compromise system safety. Direct time-of-flight (dToF) sensors address these challenges by measuring the travel time of individual photons with high precision.
This week’s New Tech Tuesdays explores the fundamentals of dToF technology, the advantages of multi-zone depth mapping, and how high-resolution optical modules enable sophisticated 3D environmental awareness.
dToF technology represents a shift from simple proximity detection to comprehensive environmental mapping. Unlike indirect methods that estimate distance based on phase shifts, a dToF sensor measures the round-trip time of light to determine how far away an object is. The reflected signal is then processed to extract depth information, and multi-zone implementations can distinguish objects at different distances within the same field of view (FOV).
Environmental robustness is another important advantage of dToF sensing. Because distance is derived from time-of-flight information using photon timestamps rather than reflected intensity alone, many dToF systems can maintain more reliable performance under challenging ambient-light conditions than simpler intensity-based optical approaches. This reliability is essential for industrial applications where dust, grease, or bright factory lighting could otherwise cause sensor failure.
The true power of modern optical sensing lies in the transition from single-point measurements to multi-zone resolution. By dividing the FOV into discrete segments, design engineers can generate a 3D depth map (Figure 1) of the surroundings rather than a single distance value. High-resolution modules now support configurable grids, such as 8×8 or 48×32, enabling granular object detection across a wide area.[1]
Figure 1: High-resolution depth mapping allows systems to visualize complex environments in 3D space. (Source: ams OSRAM)
A wider FOV, combined with a long detection range, enables systems to identify obstacles from a greater distance while maintaining peripheral awareness. In multi-zone implementations, dToF sensors can provide the spatial depth data needed for functions such as obstacle detection, host-side simultaneous localization and mapping (SLAM), cliff detection, people counting, and gesture recognition. Actual range, FOV, and spatial resolution depend on the specific device and configuration.
The ams OSRAM TMF8829 is a high-performance dToF sensor that exemplifies these imaging technological advancements in a compact 5.7mm × 2.9mm × 1.5mm module. It features a resolution of up to 48×32 pixels and can detect multiple objects per depth point simultaneously without degrading accuracy. The device provides a resolution of 0.25mm, making it suitable for both macro-range autofocus and long-range industrial automation.
To accelerate development, the TMF8829 evaluation kit provides a comprehensive platform for testing 3D depth-measurement capabilities. The evaluation software includes a graphical user interface (GUI) that visualizes 2D depth maps, 3D scatter plots, and intensity images in real time. This toolset allows design engineers to optimize sensor configurations, such as zone modes and confidence thresholds, for specific application environments.
dToF technology is redefining the possibilities of 3D depth measurement by offering unmatched precision and environmental resilience. By leveraging photon timestamps and multi-zone sensing, designers can move beyond simple proximity detection to create truly autonomous, aware systems. The ability to generate detailed depth maps over long distances with compact, low-power modules ensures that dToF sensors will remain a cornerstone of robotics, automation, and advanced consumer interfaces.
Sources
[1] https://www.mouser.com/pdfDocs/EVM.pdf
Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.