Mouser Electronics - Electronic Components Distributor
 
South Africa - Flag South Africa

Incoterms:DDU
Duty, customs fees and taxes are collected at time of delivery.

Please confirm your currency selection:

US Dollars
Free shipping on most orders over $230 (USD).
All major credit cards accepted

Euros
Free shipping on most orders over 200 € (EUR).
All major credit cards accepted

South African Rand
Free shipping on most orders over R3 800 (ZAR).
American Express not accepted as a method of payment

British Pounds
Free shipping on most orders over £170 (GBP).
All major credit cards accepted

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: Low-Power FPGAs Enable Embedded Vision at the Edge

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Embedded vision systems are evolving quickly, and with that evolution comes a shift in how designers approach system architecture. Cameras are now part of complex pipelines that include multiple sensors, interface bridges, real-time preprocessing, and edge artificial intelligence (AI) inference. As these elements converge, designers deliver more capability with smaller form factors and tighter power budgets.

Low-power field-programmable gate arrays (FPGAs) are emerging as efficient aggregation points for camera inputs and sensor data. They can bridge diverse interfaces, manage data flows, and perform early-stage processing without the overhead and latency of a full system-on-chip (SoC).

In this week’s New Tech Tuesdays, we explore how low-power FPGAs are reshaping embedded vision architectures, why they are gaining traction, and what designers can expect as edge systems continue to evolve.

From Single Sensors to Interface-Heavy Vision Systems

The growth of embedded vision is driven by demand for intelligent endpoints, from smart cameras and industrial inspection systems to human-machine interfaces (HMIs). As more processing moves to the edge, sending raw video streams to the cloud becomes less practical because of latency, bandwidth, and privacy concerns.

At the same time, sensor ecosystems have become more fragmented, requiring designers to support Mobile Industry Processor Interface Camera Serial Interface 2® (MIPI CSI-2), Universal Serial Bus (USB), low-voltage differential signaling (LVDS), and other standards within a single system. Traditionally, bridging these interfaces required multiple chips or a large SoC, increasing power consumption and design complexity.

Low-power FPGAs address this challenge by serving as flexible glue logic and preprocessing engines. Unlike fixed-function application-specific integrated circuits (ASICs) or high-power SoCs, FPGAs enable designers to customize data paths and adapt to evolving requirements without redesigning hardware. They can manage multiple input streams, synchronize sensors, and perform tasks such as image scaling or filtering while maintaining deterministic latency and low power consumption. As edge AI moves inference closer to the device, FPGA-based aggregation is bringing control and preprocessing closer to the sensor layer.

Scaling Edge Vision Without Scaling Power

As embedded vision evolves, the role of low-power FPGAs is expanding.

One trend is tighter integration with AI accelerators. FPGAs can serve as front-end processors that condition and route data efficiently into neural processing units (NPUs) or microcontrollers, reducing downstream workloads by sending selected, preprocessed data to the inference stage.

Power efficiency will also remain critical for always-on applications such as smart cameras, gesture recognition systems, and industrial monitoring devices. These use cases require architectures that remain responsive while minimizing standby and active power draw.

Another key direction is modularity and rapid prototyping. Designers need platforms that expose camera interfaces, support debugging, and allow quick iteration. System-on-module (SoM) platforms are enabling this shift by providing pre-integrated hardware blocks that accelerate development for smart endpoints and vision appliances.

Finally, scalability will continue to shape adoption. Designers need solutions that can evolve with their applications—from simple sensor aggregation to more advanced preprocessing—without requiring a complete system redesign.

The Newest Products for Your Newest Designs®

For developers building low-power embedded vision systems, the Lattice Semiconductor CrossLinkU-NX SoM board offers a flexible and efficient platform for rapid prototyping and deployment. Built around Lattice’s low-power FPGA architecture, this SoM simplifies interface-heavy designs while maintaining tight power budgets. Its low-power FPGA enables designers to aggregate and manage multiple image streams without relying on a higher-power SoC, providing efficient data routing with predictable latency and low energy consumption.

The platform also supports common vision and connectivity interfaces, making it easier to bridge disparate sensor standards within the same design. This is particularly valuable in applications that combine multiple cameras or require compatibility across evolving interface ecosystems. Combined with integrated memory and high-speed input/output (I/O), the SoM can efficiently buffer and transfer preprocessing image data in real time, helping maintain throughput in multi-sensor environments.

Tuesday’s Takeaway

Embedded vision has evolved beyond image capture to encompass the management of complex, interface-rich data pipelines at the edge. Low-power FPGAs serve as efficient aggregation and preprocessing hubs, giving designers the flexibility to build adaptable systems without sacrificing power or performance.

As edge devices continue to demand more intelligence in smaller footprints, these programmable FPGA-based solutions will play a central role in shaping the future of vision-enabled systems.

This blog was generated with assistance from Copilot for Microsoft 365.



« Back


[Post:AboutAuthor]

All Authors

Show More Show More
View Blogs by Date

Archives